Open topic with navigation
Using Matrix Tab
- Select the Matrix tab to switch the relays ON or OFF.
- Connect the instruments and devices as per your application. Key in to the available text boxes the names of the row and column for the respective port or terminal for better visual mapping.
- Click the cross-point rounded squares to toggle the relay on or off. Green means the relay is switched ON, connecting the horizontal line to the vertical line of that intersecting point. White means the relay is switched OFF, disconnecting the horizontal line from the vertical line of that intersecting point.
- When the relay that connects a row to a column is switched ON, the horizontal and the vertical lines that are connecting that row and column will be highlighted in green. When the relay that connects a row to a column is switched OFF, the horizontal and the vertical lines that are connecting that row and column will remain in white.
- Describe the colors of the relay when it is switched ON and OFF.